DOCA0180EN-08

PowerTag Link and PowerTag Link HD Gateways

PowerTag Link and PowerTag Link HD gateways are Ethernet connection concentrators (Modbus TCP/IP) for wireless devices with data display webpages.

The associated PowerTag energy sensors allow alarms to be managed through email for terminal loads, and energy, power, current, and voltage to be measured accurately in real time.

The associated PowerTag control modules are designed to monitor a circuit and to notify in wireless mode to the concentrator about the information status of a contact (OF, SD, CT, or TL position indication).

The HeatTag is a smart wireless sensor for early detection of overheating wire connections or overheating cables. It helps to prevent electrical distribution switchboards from being damaged by analyzing gas and micro-particles in the air of the switchboard and sending alerts before any smoke or insulator browning.

The PowerTag Link display is the wireless local HMI of the PowerTag system. The PowerTag Link display combined with the PowerTag Link gateway can monitor the energy locally into any electrical distribution system. The values collected by the wireless energy sensors (current, voltage, power factor, power, and energy) are displayed on the front door of your electrical panel.

To go further, the PowerTag Link display gives alarms locally. Therefore, it helps to improve your operational efficiency, and to reduce the impact of downtime.

The entire system can be easily installed in the existing low voltage equipments using Multi9, Acti9, or ComPacT NSX circuit breakers.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.