260211_MTN6185-S_SW_1842_1_0

Button Mapping

If you disable touchless function the touch buttons are active.

You can activate a maximum of 4 buttons and assign 1 function to each. The push-button has 6 areas that are activated differently, depending on the number of buttons selected.

1 button

2 buttons

3 buttons

4 buttons

By default, 4 buttons are activated and 1 function is assigned to each. The default setting is a simple assignment of the 4 functions to 4 buttons.

Button

Function

Button 1

Function 1

Button 2

Function 2

Button 3

Function 3

Button 4

Function 4

You configure the push-button in 4 steps:

  1. Define the number of buttons, from 1 to 4.

  2. Select 1 to 4 functions.

  3. Optionally, change the connection between button and function.

  4. Assign group addresses.

NOTE: If you select the Touchless function - no button, the device will not function as a button but as a touchless sensor ( refer to Touchless Function). In the next step, you will choose one of the following functions: Toggle, Switch, Time switch, Scene. You can set the parameters for each function in the Touchless function > Function menu.

You can also perform steps 2. and 3. after connecting the group addresses.

The functions are fully set.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?