DOCA0181EN-01

Smartlink SI B Gateway

The Smartlink SI B gateway has seven digital channels (24 Vdc) and one analog channel (4...20 mA or 0...10 Vdc) and can be connected to the devices in the range equipped with a Ti24 interface.

The Smartlink SI B gateway is also a wireless gateway and can be connected to wireless devices.

The data can be transmitted from the Smartlink SI B gateway to a PLC or a supervision system via a Modbus TCP/IP protocol.

The Smartlink SI B gateway channels can also be used to transmit standardized input and output. The Smartlink SI B gateway can also communicate with devices (not in the Acti9 range) with or without a Ti24 link.

The Smartlink SI B gateway is an intermediary between the supervisor and various electrical appliances. It can therefore be used to retrieve and process data received from devices, and also control them. The functions available depend on the type of connected devices.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?