DOCA0199EN-00

Smartlink SI D Gateway

The Smartlink SI D (A9XMWA20) communication system can be easily integrated into any building management architecture. It combines monitoring, metering and protection functions designed for energy efficiency solutions. Based on the Modbus protocol, the Smartlink SI D communication system allows switchboard data to be exchanged in real time with a supervision system or a PLC. The pre-wired cables of the system can save time and prevent wiring errors during installation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?