Hardware Requirements
The following hardware requirements are recommended on the PC to install the TeSys Tera DTM Library.
|
Equipment |
Minimum requirement |
Recommended requirement |
|---|---|---|
|
Processor |
Pentium 4 or Core 2 Duo, 2 GHz |
Intel® Core™ i3 |
|
RAM |
2 GB |
4 GB |
|
Display |
Resolution: 1024 x 768, 1366 x 768, 1600 x 1900, and 1920 x 1080 pixels |
Resolution: 1600 x 1900 and 1920 x 1080 pixels |
|
DPI: 96 (100%) and 120 (125%) |
DPI: 96 (100%) and 120 (125%) |
|
|
Free hard disk space on system drive |
1 GB |
2 GB |