Compatibility
The following table shows the compatibility of configuration or programming softwares with the TeSys Tera system in active releases.
| TeSys Tera firmware package version |
DTM version |
LTMTCUF control operator unit firmware version |
LTMTCUF Programmer tool version |
|---|---|---|---|
|
TeSysTera_Ethernet_V001.000.001.sedp (LTMTE••) |
DTM v2.0.0 |
TeSys Tera_HMI_V002.000.027_sedp |
Integrated to DTM |
|
TeSysTera_Ethernet_V001.000.000.sedp (LTMTE••) |
DTM v2.0.0 |
TeSys Tera_HMI_V002.000.000_sedp |
Integrated to DTM |
|
TeSysTera_Serial_V002.000.012.sedp (LTMTM•• and LTMTP••) |
DTM v2.0.0 |
TeSys Tera_HMI_V002.000.027_sedp |
Integrated to DTM |
|
TeSysTera_ V002.000.000.sedp (LTMTM•• and LTMTP••) |
DTM v2.0.0 |
LTMTCUF_HW2_V002.000.000_TERA.bin |
V3.2.000 |