DOCA0233EN-01

Status Menu

The Status Menu contains the following sub-menu:

Level 1

Level 2

Level 3

Level 4

Status Menu

IO status

DI Status

DI 1-16

DI 17-32

DO Status

DO 1-13

Trip status

Trip descriptions that can be displayed:

  • Thermal Overload

  • Stalled Rotor

  • Locked Rotor

  • DT Over Current

  • NI Over Current

  • Short Time OC

  • Calc Ground Trip

  • Meas. Ground Trip

  • Under Current

  • Current imb

  • Current ph loss

  • Current ph rev

  • Under Voltage

  • Over Voltage

  • Voltage ph loss

  • Voltage imb

  • Voltage ph rev

  • Under Freq.

  • Over Freq.

  • Under Power

  • Over Power

  • Under P.F.

  • Excessive Tstart

  • Voltage Dip

  • Max.no of start

  • Motor Stop Err Det.

  • Device Internal

  • Comm Loss

  • LTMT main unit temperature

  • DI 1 Interlock

  • DI 2 Interlock

  • DI 3 Interlock

  • DI 4 Interlock

  • DI 5 Interlock

  • DI 6 Interlock

  • DI 7 Interlock

  • DI 8 Interlock

  • DI 9 Interlock

  • DI 10 Interlock

  • DI 11 Interlock

  • DI 12 Interlock

  • HMI comm loss

  • Stucked reset key

  • Logic test interrupted

  • Motor stop error detection

Alarm status

Alarm descriptions that can be displayed:

  • Thermal Overload

  • Stalled Rotor

  • Locked Rotor

  • DT Over Current

  • NI Over Current

  • Short Time OC

  • Calc Ground Trip

  • Meas. Ground Trip

  • Under Current

  • Current imb

  • Current ph loss

  • Current ph rev

  • Under Voltage

  • Over Voltage

  • Voltage ph loss

  • Voltage imb

  • Voltage ph rev

  • Under Freq.

  • Over Freq.

  • Under Power

  • Over Power

  • Under P.F.

  • Excessive Tstart

  • Voltage Dip

  • Max.no of start

  • Motor Stop Err Det.

  • Device internal temperature

  • Comm Loss

  • LTMT main unit temperature

  • DI 1 Interlock

  • DI 2 Interlock

  • DI 3 Interlock

  • DI 4 Interlock

  • DI 5 Interlock

  • DI 6 Interlock

  • DI 7 Interlock

  • DI 8 Interlock

  • DI 9 Interlock

  • DI 10 Interlock

  • DI 11 Interlock

  • DI 12 Interlock

  • AI 1 Interlock

  • AI 2 Interlock

  • AI 3 Interlock

  • AI 4 Interlock

  • AI 5 Interlock

  • AI 6 Interlock

  • AI 7 Interlock

  • AI 8 Interlock

  • AI 9 Interlock

  • AI 10 Interlock

  • AI 11 Interlock

  • AI 12 Interlock

  • AI 13 Interlock

  • AI 14 Interlock

Inhibit status

Inhibit cause descriptions that can be displayed:

  • No Voltage

  • Under Voltage

  • Trip

  • Thermal

  • Max Starts

  • Interlock 1

  • Interlock 2

  • Interlock 3

  • Interlock 4

  • Interlock 5

  • Interlock 6

  • Interlock 7

  • Interlock 8

  • Interlock 9

  • Interlock 10

  • Interlock 11

  • Interlock 12

  • Local DI Stop

  • Remote DI Stop

  • Communication Stop

  • Forced Stop

  • Antibackspin

  • Fallback Mode Inhibit

  • Direction change

  • Speed change

  • Custom Stop

DI and DO Status Screen

The status of up to 32 digital inputs or 13 digital outputs are presented on one screen.

Example: DI 1-16 screen displays the status of 16 digital inputs on two rows:

  • First row: status of digital inputs DI 1 to DI 8, from left to right.

  • Second row: status of digital inputs DI 9 to DI 16, from left to right.

In this example, the digital input DI 2 is on, all other digital inputs are off.

  • Digital input is on

  • Digital input is off

For more information about detection of DI status, refer to the TeSys Tera Motor Management System User Guide – DOCA0257EN

Trip, Alarm, and Inhibit Status Screens

If no trip, alarm, or inhibit cause is present, None is displayed on the respective status screen.

If there is a trip, alarm, or inhibit cause, the description of that cause will be displayed on the respective status screen.

If there are more than two trip, alarm, or inhibit causes, you can use the and to scroll through the descriptions of each cause. The descriptions are not presented in chronological order.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.