Installation Instructions for the IMD Version
-
ERMS/ERM2 I-LEM Installation Position
-
Following the instructions in I-Line Enable Module Instruction Bulletin (JYT97577), the ERMS/ERM2 I-LEM (item 3, of Front View of FlexSeT Switchboard with ERMS Feature: I-Line Stack Location of ERMS/ERM2 I-LEM) is factory installed in the lowest position of the I-Line section. The wire harness provided in the FlexSeT switchboard adjacent section is suitable for this location only.
-
-
Wire Harness Routing
-
Locate the harness to be installed in the main breaker section. See Shipping Location of Pre-Assembled Wire Harness.
-
Uncoil the pre-assembled harness to extend the length while maintaining the integrity of the factory pre-assembled portion.
-
Identify and cut off the coiling/fixing wire-ties using suitable wire snips. Be careful not to cut off the wire-mount dedicated wire ties. See Shipping Location of Pre-Assembled Wire Harness.
-
Pass the harness underneath the section vertical barrier (item 1 of Detailed View of Wire Harness Installation in the FlexSeT Switchboard) to extend and reach the I-LEM (item 3 of Detailed View of Wire Harness Installation in the FlexSeT Switchboard and Final Wire Mounts and Plug Connections to ERMS/ERM2 I-LEM). Secure the wire harness using the harness pre-installed adhesive mount (item 2 of Detailed View of Wire Harness Installation in the FlexSeT Switchboard) and the three push-in wire mounts (items 4, 5 and 6 of Detailed View of Wire Harness Installation in the FlexSeT Switchboard and Final Wire Mounts and Plug Connections to ERMS/ERM2 I-LEM) within the I-Line section. Gently adjust the push-in wire mount positions along the harness length to provide a neat and professional appearance. Ensure that the wire mounts align to the specified position and matching holes.
-
Connect the 24 Vdc harness 2-Pin connector (item 8 of Final Wire Mounts and Plug Connections to ERMS/ERM2 I-LEM) to the ERMS/ERM2 I-LEM port labeled as "DC POWER OUTPUT / 24V+ 24V-" (item 9 of ERMS/ERM2 I-LEM Panel for Plug Connection).
-
Connect the ULP (Universal Logic Plug) RJ45 type connector (item 7 of Detailed View of Wire Harness Installation in the FlexSeT Switchboard) to the port labeled as "ULP 1" (item 10 of ERMS/ERM2 I-LEM Panel for Plug Connection) on the ERMS/ERM2 I-LEM. Ensure that the correct ULP and 24 Vdc plug connectors are used and connected to the designated ports on the ERMS/ERM2 I-LEM.
-
-
Perform all functional ERMS tests per the Energy Reduction Maintenance Setting (ERMS) System Installation and User Guide (NHA67346).