Cable-lug Adapter

Cable-lug adapters are used to adapt the cable lug connection on vertical connection adapters of the TransferPacT Active Automatic 800–1600 A Transfer switching equipment.

Cable-lug adapters are screwed on the switch using the screws delivered with the cable-lug adapters.

The table below provides the list of the vertical connection adapter:

Switch

Number of poles

Vertical connection adapter

Frame 1A: 800–1600 A

3P

33644 / LV833644SP

4P

33645 / LV833645SP

For information on installation, consult the instruction sheet on the Schneider Electric website: BQT7680301 .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?