Overview

The mechanism accessories for the TransferPacT Active Automatic, TransferPacT Automatic and TransferPacT Remote are as below:

  • Power connection accessories
    • Steel connectors

    • Aluminum connectors

    • Linergy DP distribution block

    • Vertical connection adapters

    • Terminal extensions

    • Spreaders

    • Load extension bars

    • Cable lug adapters

    • Copper/aluminum lugs

  • Insulation accessories
    • Terminal cover

    • Interphase barriers

    • Terminal shields

    • Insulating screens

    • PowerTag

  • Auxiliary contacts

  • Upside down installation kit

  • Spare parts

    • Handles

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?