Switch Accessories

Accessories for the switch are as below:

  • OF auxiliary contacts (wired) (TPSAUX32, TPSAUX33, TPSAUX43, TPSAUX44, TPSAUX71, TPSAUX72)

  • Power connection accessories

    • Steel connectors (LV429242, LV429243)

    • Aluminum connectors (LV429227, LV429228, LV429259, LV429260, TPSCON47, TPSCON48, TPSCON49, TPSCON50, TPSCON51, TPSCON52, TPSCON53, TPSCON54)

    • Bare cable connectors (33640, 33641)

    • Vertical connection adapters (33642/LV833642SP, 33643/LV833643SP)

    • Straight terminal extensions (LV429263, LV429264)

    • Edgewise terminal extensions (LV429308, LV429309, TPSCON55, TPSCON56)

    • Spreaders (LV431563, LV431564, TPSCON39,TPSCON40, TPSCON41, TPSCON68, 33622/LV833622SP, 33623/LV833623SP)

    • Load extension bars (TPSCON35, TPSCON36)

    • Compression lug (LV429252, LV429253, LV429254, LV429256, LV429257, LV429258, LV429504, LV429505, LV429506, LV429507, TPSCON57, TPSCON58, TPSCON59, TPSCON60, TPSCON61, TPSCON62, TPSCON63, TPSCON64)

    • Cable-lug adapters (33644/LV833644SP, 33645/LV833645SP)

    • Linergy DP distribution block (LVS04033, LVS04034)

  • Insulation accessories

    • Interphase barrier (TPSISO29, TPSISO65, TPSISO70)

    • Terminal shield (TPSISO30, TPSISO31)

    • Long terminal shield (LV429518, TPSISO42)

    • Insulating screen (TPSISO66, TPSISO67)

  • Monitoring accessories

    • PowerTag (LV434021)

  • Upside down installation kit (TPSOTH73)

  • Handle (TPSOTH69)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?