Terminal Extension

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
  • It is mandatory to install interphase barriers when terminal extensions are used.
  • For straight terminal extensions, it is mandatory to install insulating screen or custom made fiber insulating plate.
Failure to follow these instructions will result in death or serious injury.

The terminal extensions are used to extend the connection possibilities of the switch.

The terminal extensions are screwed on the switch using the screws delivered with the terminal extensions.

The table below provides the list of the straight terminal extension:

Switch

Number of poles

Straight terminal extensions

Frame 250: 100–250 A

3P

LV429263

4P

LV429264

The table below provides the list of the edgewise terminal extension:

Switch

Number of poles

Edgewise terminal extensions

Frame 250: 100–250 A

3P

LV429308

4P

LV429309

Frame 630: 320–630 A

3P

TPSCON55

4P

TPSCON56

For information on installation, consult the instruction sheets on Schneider Electric website:

  • TransferPacT Active Automatic / Automatic / Remote 100–250 A: GEX2525501

  • TransferPacT Active Automatic / Automatic / Remote 320–630 A: GEX2525601

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?