Accessories

External HMI Accessories

Accessories for the external HMI are as below:

  • External HMI for Active Automatic HMI (TPCCIF04)

  • External HMI cable (TRV00810, TRV00820, TRV00830)

  • IP 54 cover (TPCOTH37 / TPCOTH38)

Controller Function Modules

The options and spare parts are:

  • Load shedding and availability warning (TPCDIO05)

  • Genset start and alarm (TPCDIO17)

  • Transfer inhibit and remote testing (TPCDIO07)

  • Voluntary remote control (TPCDIO08)

  • Fire protection

    • 24 V DC pulse (TPCDIO10)

    • 24 V DC constant (TPCDIO11)

    • 230 V AC constant (TPCDIO13)

    • 1 dry contact (TPCDIO14)

  • BUS extension and 24 V DC auxiliary supply (TPCDIO15)

    • 24 V+ and 24 V- DC port

    • RJ45

  • Modbus RTU (TPCCOM16)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?