TPCDIO15: BUS Extension and 24 V DC Auxiliary Supply

Wiring

Terminal

NOTE:
  • TPCDIO15 is used only for TransferPacT Active Automatic.

  • To get the best performance, TPCDIO15 need to install on the rightmost slot of frame 100, 160 and 1A, and on the top slot of frame 250, 630 and 800.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?