Event Logs

TransferPacT ATSE can record maximum up to 99 events of the event logs. If it exceeds the events limit, the latest logs will overwrite the previous event logs. The limit of event logs on LCD and Modbus are:

  • LCD can only display the last 20 events.

  • Modbus can display all the events.

Perform the following procedure to check the event logs:

  1. Select the Status page from Home page and press OK button.

  2. Select Event Logs option and press OK button.

  3. Select SI Back To Normal.

  4. Press OK button to check the selected event log.

Event Logs Page Description

Label

Description

1

Time of events.

NOTE: Without any time calibration or external DC 24 V, after long terms shut down of controller, the timer may show wrong.

2

The source status during the events.

3

Code of events.

4

Transfer mode during the events.

NOTE: Event logs cannot be reset.

List of Event Logs

Event Code

LCD Display

1

Position alarm: Transfer to A Failed

2

Position alarm: Transfer to N Failed

3

Position alarm: Transfer to OFF Failed

4

Position alarm: Transfer to Invalid Position

5

Position Alarm: Internal Error

6

Position alarm: Unexpected position

10

SI Phase Rotation Error

11

SII Phase Rotation Error

12

Unsupported Device RS Alarm

30

Genset Invalid

31

Genset Start Failure

40

On Load Test Failure

41

Off Load Test Failure

42

On Load Test Success

43

Off Load Test Success

50

SI Unbalance Warning

51

SII Unbalance Warning

52

SI Neutral Position Wrong Warning

53

SII Neutral Position Wrong Warning

54

SI Neutral Loss Warning

55

SII Neutral Loss Warning

70

SI Undervoltage

71

SII Undervoltage

72

SI Overvoltage

73

SII Overvoltage

74

SI No Voltage

75

SII No Voltage

76

SI Underfrequency

77

SII Underfrequency

78

SI Overfrequency

79

SII Overfrequency

80

SI All Recover

81

SII All Recover

100

SI Voltage over 500 V

101

SII Voltage over 500 V

120

Transfer from N to A

121

Transfer from A to N

122

Transfer from N to O

123

Transfer from A to O

124

Transfer from O to N

125

Transfer from O to A

140

Load Shedding Output

141

Genset Start

142

Genset Stop

143

Alarm Output Start

144

Alarm Output Stop

145

Force to OFF

146

Fire Start

147

Fire Stop

148

Enter Inhibit Mode

149

On Load Test

150

Off Load Test

151

Voluntary to N

152

Voluntary to A

153

Comm Transfer Exit

154

Comm Transfer to N

155

Comm Transfer to A

156

Comm Transfer to OFF

200

Operation Mode Changed

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?