Quickview Page

  1. Select Quick View and press OK button to open its sub-pages.

  2. Press Up and Down buttons to navigate to each sub-page.

The below table provide the details of the Quick View sub-pages:

Sub-page name

Sub-page function

Display

System Overview

To show the system overview:

  • SI and SII general status.

  • Contact position.

SI

To show the SI voltage status:

  • Real time phase voltage of SI.

  • Real time frequency of SI.

SII

To show the SII power status:

  • Real time phase voltage of SII.

  • Real time frequency of SII.

Slots

To show the slot status:

  • Black box indicates that the accessories are working.

  • Empty box indicates that the accessories are not working.

Date / Time

This sub page is to show the timer in controller.

NOTE: Calibrate the timer after long terms of power interruption. Use DC 24 V to keep the accuracy of the timer.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?