Warning

When the warning is triggered for event codes, such as 30,31,40,41,50,51,52 and 53, the HMI will pop-up the alarm screen. The green source LED blinks OFF or ON for event codes such as 54,55,70,71,72,73,74,75,76,77,78,79,80 and 81. The event code list and display method are shown in the below table.

The icon is displayed on the page to indicate an active warning.

If the warning is triggered, it will display the latest warning and previous alarms are overwritten on the HMI. The log will be recorded.

Perform the following procedure to check and clear the alarm:

  1. Select the Set & Operate page and press OK.

  2. Enter the password to open the Set & Operate page.

  3. Select Operations sub-page.

  4. Press Down button and select Warning Ack.

  5. Click OK on the screen.

The warning will not inhibit the transfer functions for the below event codes:

List of Event Codes

Alarm code

Alarm message

LCD display method

LED display method

30

Genset invalid

Bottom bar

None

31

Genset start failure

Bottom bar

None

40

On load test failure

Bottom bar

None

41

Off load test failure

Bottom bar

None

42

On load test success

Bottom bar

None

43

Off load test success

Bottom bar

None

50

SI unbalance warning

Bottom bar

None

51

SII unbalance warning

Bottom bar

None

52

SI neutral position wrong warning

Bottom bar

None

53

SII neutral position wrong warning

Bottom bar

None

54

SI neutral loss warning

None

LED source state blinking

55

SII neutral loss warning

None

LED source state blinking

70

SI under voltage

None

LED source state blinking

71

SII under voltage

None

LED source state blinking

72

SI over voltage

None

LED source state blinking

73

SII over voltage

None

LED source state blinking

74

SI no voltage

None

LED source state off

75

SII no voltage

None

LED source state off

76

SI under frequency

None

LED source state blinking

77

SII under frequency

None

LED source state blinking

78

SI over frequency

None

LED source state blinking

79

SII over frequency

None

LED source state blinking

80

SI all recover

None

LED source state on

81

SII all recover

None

LED source state on

SI Unbalance Warning

  • Event code: 50.

  • Type of event: Warning.

  • Default: Disable.

  • Description: If unbalance of voltage occurs over the drop-out rate of threshold (5% as default) when SI is connected, a warning will be raised.

  • Cause: Too many single-phase loads or poor quality of power supply environment.

  • Diagnosis and repair: Set the different value of imbalance rate or contact field service.

SII Unbalance Warning

  • Event code: 51.

  • Type of event: Warning.

  • Default: Disable.

  • Description: If unbalance of voltage occurs over the drop-out rate of threshold (5% as default) when SII is connected, a warning will be raised.

  • Cause: Too many single-phase loads or poor quality of power supply environment.

  • Diagnosis and repair: Set the different value of imbalance rate or contact field service.

Generator Invalid

  • Event code: 30.

  • Type of event: Warning.

  • Default: Always disable.

  • Description: The sudden loss of an alternate source will lead to a warning.

  • Cause: Genset is not connected well or some failure on Genset started

  • Diagnosis and repair: Contact field service.

Generator Start Failure

  • Event code: 31.

  • Type of event: Warning.

  • Default: Disable.

  • Description: After sending the Genset start signal, controller will wait a time T10 duration until Genset is ready.

    • The ATSE will rise the Genset alarm, if Genset is not started within T10 timer is ended (if enabled).

    • The ATSE shall reset the Genset alarm, when the A source is in range or when the N source is in range.

    • The time delay is only available when there is external power.

  • Cause: Genset is not connected well or some failure on Genset started.

  • Diagnosis and repair: Contact field service.

On Load/Off Load Test Failure

  • Event code: 40, 41

  • Type of event: Warning.

  • Default: Always enabled.

  • Description: If on load or off load test is failed or interrupted, a warning will be raised.

  • Cause: Product failure or external interruption

  • Diagnosis and repair: Contact field service.

SI or SII Neutral Position Wrong Warning

  • Event code: 52, 53

  • Type of event: Warning.

  • Default: Always enabled in IEC market, disabled in China market.

  • Description: If sequence of neutral is not connected as set value, a warning will be raised.

  • Cause: Wrong connection of neutral or wrong settings.

  • Diagnosis and repair: Set the new neutral sequence or contact field service.

SI or SII Neutral Loss Warning

  • Event code: 54, 55

  • Type of event: Warning.

  • Default: Disabled.

  • Description: If unbalance rate of voltage occurs over 20% when source is connected, a warning will be raised.

  • Cause: Miss connection or disconnection caused by interior or exterior impacts of neutral line..

  • Diagnosis and repair: correct the connection or contact field service.

SI Under Voltage

  • Event code: 70.

  • Type of event: Event.

  • Default: Always enable.

  • Description: When there is under voltage on SI, an event log will be recorded.

SII Under Voltage

  • Event code: 71.

  • Type of event: Event.

  • Default: Always enable.

  • Description: When there is under voltage on SII, an event log will be recorded.

SI Over Voltage

  • Event code: 72.

  • Type of event: Event.

  • Default: Disabled.

  • Description: When there is over voltage on SI, an event log will be recorded.

SII Over Voltage

  • Event code: 73.

  • Type of event: Event.

  • Default: Disabled.

  • Description: When there is over voltage on SII, an event log will be recorded.

SI No Voltage

  • Event code: 74.

  • Type of event: Event.

  • Default: Always enable.

  • Description: When there is source failure on SI, an event log will be recorded.

SII No Voltage

  • Event code: 75.

  • Type of event: Event.

  • Default: Always enable.

  • Description: When there is source failure on SII, an event log will be recorded.

SI Under Frequency

  • Event code: 76.

  • Type of event: Event.

  • Default: Disable

  • Description: When there is Under frequency on SI, an event log will be recorded.

SII Under Frequency

  • Event code: 77.

  • Type of event: Event.

  • Default: Disable

  • Description: When there is Under frequency on SII, an event log will be recorded.

SI Over Frequency

  • Event code: 78.

  • Type of event: Event.

  • Default: Disable

  • Description: When there is Under frequency on SI, an event log will be recorded.

SII Over Frequency

  • Event code: 79.

  • Type of event: Event.

  • Default: Disable

  • Description: When there is Under frequency on SII, an event log will be recorded.

SI All Recover

  • Event code: 80.

  • Type of event: Event.

  • Default: Always enable.

  • Description: When SI recover to normal, an event log will be recorded.

SII All Recover

  • Event code: 81.

  • Type of event: Event.

  • Default: Always enable.

  • Description: When SII recover to normal, an event log will be recorded.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?