Overview

The control mode is used to operate TSE in different applications. The TransferPacT Active ATSE contains every function needed with nine control modes:

  • Auto mode

  • Test mode

  • Communication transfer mode

  • Voluntary transfer mode

  • Local control mode

  • Transfer inhibit mode

  • Fire protection mode

  • Force to off mode

  • Handle transfer mode


The TransferPacT Automatic contains below control modes:

  • Auto mode

  • Test mode

  • Voluntary transfer mode

  • Transfer inhibit mode

  • Fire protection mode

  • Force to off mode

  • Handle transfer mode

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?