Overvoltage Thresholds

Field

Description

Default value

  • Dropout: 10%

  • Pickup: 20% of delta dropout

Range

Delta voltage ranges from 4%–20% of rated voltage: It could be 4–6–8–10–12–14–16–18–20%.Default value: 10%

Differential

The differential between dropout and pickup on automatic HMI is fixed. The differential is set at 20% of the delta value.

Sequence of events

  • When a sensor detects a voltage below the dropout set voltage for a period longer than the time delay, it will deem the voltage for out of range.

  • When a sensor detects a voltage at or above the pickup point, it will deem the voltage as applicable.

Example of calculation on overvoltage of TransferPacT Automatic

For example, Ue= 400 V , Dropout 10%= 40 V,

Differential between dropout and pickup= 40 V * 20%= 8 V

overvoltage dropout is 400 V + 40 V= 440 V

Pickup= 440 V - 8 V= 432 V

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?