Time Delay

-

Adjust

Range

Default

Symbol

Display

Definition

Active automatic

Active automatic

Active automatic

T2

Transfer Delay

Confirmation delay on source power failure

0.1 s from 0-1 s. 1 s when >1 s.

0-1800 s

3 s

T4

Center-off Delay

OFF position delay

1 s

0-30 s

0 s

T6

Re-transfer Delay

Confirmation delay to re-transfer on normal source

1 s

0-3600 s

60 s

T7

Genset Start Delay

Delay to start Genset

1 s

0-120 s

3 s

T8

Loadshed Delay

Delay to load shedding

1 s

0-15 s

0 s

T9

Genset cool delay

Genset cooling down delay

1 s

0-3600 s

60 s

T10

Genset fail delay

Genset alarming failure detection time

1 s

15–300 s

300 s

T13

On load test delay

Time duration to run for test process on load.

1 s

Unlimited: 0 s

Limited: 1-1800 s

Unlimited: 0 s

Limited: 30 s

T14

Off load test delay

Time duration to run for test process off load.

1 s

Unlimited: 0 s

Limited: 1-1800 s

Unlimited: 0 s

Limited: 30 s

T2: Transfer Delay

Field

Description

Applications

  • Confirm connected source has failure.

  • Measure the target source power (for example voltage and frequency) during the time delay.

  • The delay shall detect both sources, the stop condition will be N recovered, or A source failed.

Default values

3 s

Range

0–1800 s

Adjust

Step of 0.1 s from 0-1 s. 1 s when >1 s.

T4: Center-Off Delay

Field

Description

Applications

  • Time delay applied to the center-off position O when Position I and Position II are transferring, it stops at Position O to protect inductive load.

  • The delay is used for both process of transfer to N and A.

Default values

0 s

Range

0–30 s

Adjust

Step of 1 s

T6: Re-Transfer Delay

Field

Description

Applications

  • Time delay applied when transferring from R to N in the Auto-Return mode. This delay is intended to measure the N and R during the delay.

  • If N is abnormal, the timer will stop and the re-transfer is cancelled.

  • If R is abnormal but Source N is normal, the switch will transfer immediately.

Default values

60 s

Range

0–3600 s

Adjust

Step of 1 s

T7: Genset Start Delay

Field

Description

Applications

  • Genset startup time delay (time delay before sent the signal to start Genset), available for U-G applications.

  • The time delay only available when there is external power or select the Genset start module.

Default values

3 s

Range

0–120 s

Adjust

Step of 1 s

T8: Loadshed Delay

Field

Description

Applications

  • Load shedding delay, for U-U/U-G.

  • Load shed: The alternate power (Genset) sometimes may not afford all loads. A signal from controller will shed some loads.

  • Need customer to decide which load can be shed.

Default values

0 s

Range

0–15 s

Adjust

Step of 1 s

T9: Genset Cool Delay

Field

Description

Applications

  • Delay between closing of N source and send the signal to stop the Genset.

  • The propose is to keep the generator running at no load for some time before shutting / cooling down.

  • When controller restarts, this time delay will be running also at U-G mode.

NOTE: To prevent any risk of Genset damage due to Genset stopping before the end of its starting process: Genset cooling time delay can only start after the end of Genset start time delay or after SII is within tolerances since source return time delay.

Default values

60 s

Range

0–3600 s

Adjust

Step of 1 s

T10: Genset Fail Delay

Field

Description

Applications

  • After sending the Genset start signal, controller will wait a time duration T10 until Genset is ready.

  • The ATSE shall rise the Genset alarm, if genset is not started while T10 timer is ended (if enabled).

  • The ATSE shall reset the Genset alarm, when the R source is in Range or when the N source is in Range.

  • The time delay is only available when there is external power.

Default values

  • The default value is 300 s.

  • The alarm can be enabled or disabled. Default as disabled.

Range

15–300 s

Adjust

Step of 1 s

T13: On Load Test Delay

Field

Description

Applications

Time duration for On load test process. It will rise the alarm if test is not finished in the time duration.

Default values

  • Default as unlimited(0 s), has to manual stop test procedure.

  • If select limited, default as 30 s.

Range

1–1800 s

Adjust

Step of 1 s

T14: Off Load Test Delay

Field

Description

Applications

Time duration for off load test process. It will rise the Alarm if test is not finished in the time duration.

Default values

  • Default as unlimited(0 s), has to manual stop test procedure.

  • If select limited, default as 30 s.

Range

1–1800 s

Adjust

Step of 1 s

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?