Wizard Setup

NOTE: The transfer function of TransferPacT ATSE is available only after configuring wizard setup.

A Wizard should be configured once the ATSE is power ON for the first time.

Perform the following procedure to complete the wizard setup:

  1. Select the language.

    There are eight languages and options are:

    • English

    • French

    • Spanish

    • German

    • Italian

    • Portuguese

    • Russian

    • Chinese

  2. Select the Rated Voltage.

    The rated voltages options are:

    • 2P: 220 V, 230 V, 240 V, 250 V

    • 3P and 4P: 380 V, 400 V, 415 V, 440 V

    NOTE: The power supply of TransferPacT is required to be 380 V AC - 20% to 440 V AC + 20% at a frequency of 50/60 Hz and it has been developed to meet most of the network configurations.

  3. Select the Rated Frequency.

    The rated frequencies options are:

    • 50 Hz

    • 60 Hz

  4. Select the Neutral Position.

    The neutral position options are:

    • A-B-C-N

    • N-A-B-C

  5. Select the Source Configuration.

    The different source type and priority is shown below:

    • SI-Utility(N)/SII-Utility(A)

    • SI-Utility(N)/SII-Genset(A)

    • SI-Genset(A)/SII-Utility(N)

    • SI-Utility(A)/SII-Utility(N)

  6. Select the Return Modes.

    The return modes options are:

    • Auto-Return

    • Non-Return

  7. Click OK to save the changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?