System Parameters Sub-Page

The below table provide the details of the System Parameters sub-pages:

Sub-page name

Sub-page function

Display

System Param

Set & Operate page navigates to more maintenance options in the display and click System Param to set nominal values.

System Param page navigates to more parameter options

Rated Voltage

Rated Voltage is a sub-page of System Param.

Click Rated Voltage to set nominal values of voltage.

Navigate to select different rate voltage:

  • 2 P : 220 V, 230 V, 240 V, 250 V

  • 3 P and 4 P: 380 V, 400 V, 415 V, 440 V

Confirm Operation

Confirm Operation window is to confirm the Rated Voltage and click OK to save changes.

Rated Frequency

Rated Frequency is a sub-page of System Parameters.

Click Rated Frequency to set nominal values of frequency.

Navigate to select different rated frequency:

  • 50 Hz

  • 60 Hz

Confirm Operation

Confirm Operation window is to confirm the Rated Frequency and click OK to save changes.

Neutral Position

Neutral Position is a sub-page of System Param.

Click Neutral Position to set nominal values of Neutral Position.

Navigate to select different neutral position:

  • A-B-C-N

  • N-A-B-C

Confirm Operation

Confirm Operation window is to confirm the Neutral Position and click OK to save changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?