Time Delays Sub-Page

The below table provide the details of the Time Delays sub-pages:

Sub-page name

Sub-page function

Display

Time Delays

Set & Operate page navigates to more maintenance option in the display and click Time Delays to set transfer times delay for different application.

Transfer Delay

Transfer Delay is a sub-page of Time Delays.

Click Transfer Delay to set transfer delay and click OK.

  • Use up or down button to set it. The range of transfer time is from 0-1800 s with step of 1 s.

  • Default value is 0 s.

Confirm Operation

Confirm Operation window is to confirm the Transfer Delay and click OK to save changes.

Re-Transfer Delay

Re-Transfer Delay is a sub-page of Time Delays.

Click Re-Transfer Delay to set re-transfer delay and click OK.

  • Use up or down button to set it. The range of re-transfer time is from 0-3600 s with step of 1 s.

  • Default value is 0 s.

Confirm Operation

Confirm Operation window is to confirm the Re-Transfer Delay and click OK to save changes.

Center-off Delay

Center-off Delay is a sub-page of Time Delays.

Click Center-off Delay to set center-off delay and click OK.

  • Use up or down button to set it. The range of centre off delay is from 0-30 s with step of 1 s.

  • Default value is 0 s.

Confirm Operation

Confirm Operation window is to confirm the Center-off Delay and click OK to save changes.

Loadshed Delay

Loadshed Delay is a sub-page of Time Delays.

Click Loadshed Delay to set load shedding delay and click OK.

  • Use up or down button to set the value.

  • The range of load shedding delay is from 0-15 with step of 1 s.

  • Default value is 0 s.

Confirm Operation

Confirm Operation window is to confirm the Loadshed Delay and click OK to save changes.

Genset Start Delay

Genset Start Delay is a sub-page of Time Delays.

Click Genset Start Delay to set genset delay and click OK.

  • Use up or down button to set it. The range of genset start time is from 0-120 s with step of 1 s.

  • Default value is 0 s.

Confirm Operation

Confirm Operation window is to confirm the Genset Start Delay and click OK to save changes.

Gen Cool Delay

Gen Cool Delay is a sub-page of Time Delays.

Click Gen Cool Delay to set genset cooling down delay and click OK.

  • Use up or down button to set it. The range of genset cooling down delay is from 0 to 3600 s with step of 1 s.

  • Default value is 60 s.

Confirm Operation

Confirm Operation window is to confirm the Gen Cool Delay and click OK to save changes.

Gen Fail Delay

Gen Fail Delay is a sub-page of Time Delays.

Click Gen Fail Delay to set genset ready alarm delay and click OK.

  • Genset failure delay is from 0 ~300 s. Default value is 300 s.

  • Use up or down button to set it.

  • The range of genset ready alarm is from 0-15 with step of 1 s.

  • Default value is 0 s.

NOTE: This function of genset ready alarm can be disabled.

Confirm Operation

Confirm Operation window is to confirm the Gen Fail Delay and click OK to save changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?