Home Page of LCD Display

Label

Description

Function

1

Quick View

Name for current page

2

Quick View

Open Quickview menu to check general information of ATSE

3

Set & operate

Open Set & operate menu for commissioning and settings

4

Measure

Open Measure menu to check the details of power status

5

Status

Open Status menu to check status of ATSE include event logs

6

Icon for time

To show the time

7

Time

Time which needs to be reset after power contingency

8

Transfer Mode

Eight control modes:

  • Auto mode (AT)

  • Test mode

  • Comm mode

  • Voluntary transfer mode

  • Local control mode

  • Transfer Inhibit mode

  • Force to off mode

  • Fire protection mode

  • Handle transfer mode

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?