Commissioning the Hub and Basic Hub gateway (Ethernet mode)

If the hub and Basic Hub gateway is connected to the network by Ethernet, commissioning involves adding the hub gateway to the Home using the app.

Before commissioning the hub gateway, the hub gateway must be connected to the Wi-Fi network router using an Ethernet cable. (See Connecting the hub gateway to the Wi-Fi network Connecting the Basic Hub to the Wi-Fi network.) After commissioning, you can optionally switch the connection to Wi-Fi, if needed. (See Switching the SmartHUB hub gateway Ethernet connection to Wi-Fi (optional).)

NOTE: Before commissioning the hub gateway, make sure that both the hub gateway and mobile phone are connected to the same Wi-Fi network router.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?