Ethernet mode connection- SmartHUB Wiser Hub Gateway

  1. Locate the Ethernet port (A) on the ELKO SmartHUB hub gateway.
  2. Connect an Ethernet cable between the SmartHUB hub gateway and the router to suit the installation method used for the SmartHUB hub gateway:
    • Wall box installation (B)

    • Wall mount using two screws (C)

    • Wall mount using two screws (B)

    • Table mount using optional tablestand (C)

    • Table mount using optional Docking Kit (D)

You must add the SmartHUB hub gateway to the app before you can add devices to control them. To do this, first download and install the app on your mobile phone/tablet (see Downloading the app Downloading the app ) and register a user account. You can then add the hub gateway and optionally connect the SmartHUB hub gateway to the network router by Wi-Fi.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?