DUG_Wiser IPC_Indoor_LK-01

Using patrol mode

The patrol mode allows you to set up movements for camera to scan a large area by rotating the camera in a single continuous path automatically.
To turn on the patrol mode:
  1. On the Home page, tap All devices > IP Camera Indoor.
  2. Tap > Settings.
  3. Tap the toggle switch to turn on the Patrol Mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?