DUG_Exxact_SSO_WSE_00

Renaming the device

You can rename the device using the Wiser app.
  1. On the Home page, select the device for which you wish to rename.
  2. At the top-right corner of the screen, tap .
  3. Tap edit next to the device name.
  4. Tap Name, enter the new name (A) and then tap Confirm.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?