Calibrating Shutter Blinds

The device is supplied in an uncalibrated state.

Each shutter blinds motor varies in the time taken to complete the movement from bottom to top position (i.e. edge to edge). This is called the run time.

To determine the default time, operate the Shutter blinds and use a stopwatch to record the time it takes to move from fully closed to the fully open position.

In the app, enter the recorded time in seconds in the drive time section of the device Settings page.

NOTE: The default run time is 120 s.

When the shutter blinds is operated for the first time after the drive time is set, the shutter blinds performs a calibration by completing a full movement from edge to edge. The Green LED turns off and then shutter blinds drives to the desired position.

IMPORTANT: Do not use the shutter blinds while the calibration is in process to avoid any interruption.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?