EcoWatt
It gives out 3 different levels of status, at the national level, updated every hour, with 48 hours forecast data. EcoWatt allows you to know the moments when eco-gestures have the greatest impact on the electrical system.
-
Send notifications about the grid status.
-
Send alerts if there is a risk of power cut.
-
Provides eco-gestures to consume better electricity.
-
Helps to save electricity during periods of high consumption.
-
Allows to view daily electricity consumption impacted by weather.
-
Helps to reduce energy consumption and avoid critical tension on Grid.
Once the Wiser Home app is updated, user gets notified that this feature is available. The Ecowatt screen appears on the Home screen.
-
Read the feature update and swipe to navigate to next screen.
-
Tap
to close the overlay screen.
Any one of the following National Electrical Grid status appears on the Home screen:
-
Green (A):
The electrical grid is operating normally. -
Amber (B):
The electrical grid is tensed and eco-gestures are highly recommended. -
Red (C):
The electrical grid is tensed and there is not enough electricity to fulfill France’s needs. Everyone should reduce their consumption.
Tap the National Electrical Grid status. In this example (B) is selected.
-
-
The forecast and eco-gesture details are shown. Tap (D) or swipe to navigate between days.
-
Scroll down to view the devices that can be consumed at the best time and energy saving tips (E).
-
Follow the eco-gestures based on the grid status (amber or red) that apply to your home to consume better electricity. Example, turning off unnecessary lights, lowering, the heating temperature to 19°C.
Setting EcoWatt alerts
You can set the alert type of your choice.
Disabling EcoWatt status
You can disable the EcoWatt status on the Home screen if not required.
-
Tap the toggle switch (A).
A notification window is prompted.
-
Tap OK on the notification window.
NOTE: You can enable the toggle switch whenever required.
After you disable this feature, you can still get tips from push notifications, but you don't have the status displaying in the Home screen. This is a reminder that you've disabled the feature.