DUG_LK FUGA Wiser wireless PIR with relay_WH-00

Configuring the device

The Device Details screen allows you to configure the Motion Sensor Switch according to your preferences.
  1. On the Home screen, tap .

  2. Tap Devices > Lights > Motion Switch to locate the Device Details screen.

A

Device Name: Tap to change the name of the device.

B

Location: Tap to assign the device to any room (such as living room, bedroom, kitchen etc). For more information, refer to Setting the device location.

C

Motion Detection Sensitivity: Tap to set the sensitivity level of the sensor as per your preference. For more information, refer to Setting the detection sensitivity for detailed information on each option.

D

Motion Detection Timer: Tap to set the time for how long the light should remain On after motion is detected. For more information, refer to Setting the motion detection timer.

E

Current Lux: Displays the current Lux value of the light present in the environment measured by the sensor. Lux is a unit of illuminance that measures the amount of visible light present in an area. It helps the sensor determine how bright or dark the environment is.

F

Lux Level Threshold: Tap to set the threshold value for Lux ranges that determine when the sensor should activate. For more information, refer to Defining Lux settings.

G

Notify me if motion is detected: Tap the toggle switch to receive notifications when motion is detected.

H

Identify: Tap to identify the device. The status LED blinks red and the connected light blinks on and off, upon successful identification.
Tap OK when you finish identifying the device.

I

Delete: Tap to remove the device from the system.

NOTE:
  • Removing the device will also reset the device. After reset, the LED turns amber indicating that the device is ready for pairing.

  • If there is a problem while pairing or resetting the device, refer to Resetting the device.

J

Zigbee Signal Strength Indicator: Zigbee Signal Strength indicator which displays the current signal strength of the device.

  • Good Signal (between 0 & -54dBm)

  • Normal Signal (between -54 & -79dBm)

  • Poor Signal (<-79dBm)

  • No Signal (device is offline)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.