DUG_Odace Shutter_WH-07

Shutter Calibration without Wiser app

To set the calibration without Wiser app:
  1. Remove the rocker from the Blind control switch.

    NOTE: Removing the rocker helps to use both top and bottom push-buttons together. Without removing the rocker, you can use either top or bottom push-button.

  2. Press bottom and top push-buttons for 3 seconds.

    The status LED blinks green.

    • If the shutter is not in a completely open position, it starts to open and reaches the top position.

    • In this step, If the shutter is already in the open position, then there will be no movement of the shutter.

    NOTE: LED blinks green throughout the calibration process.

  3. Short press the top push-button when the shutter opens completely.

    The shutter starts to close and reaches the bottom position.

  4. When the shutter reaches the bottom position, immediately press the top push-button once.

    The shutter starts to open and reaches the top position.

  5. When the shutter reaches the top position, immediately press the top push-button once.

    Shutter starts to move and automatically reaches a middle position to finish the calibration.

    NOTE: The exact shutter position depends on the shutter type, motor and mechanical construction. Based on this, the middle position will differ.

  6. Reassemble the rocker on the Blind control switch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?