Showing 111 - 120 of 1,457 results

Page 12 of 146
  • Understanding Control Mode Priorities

    Wiser Home – System User Guide (Denmark)

    any pre-existing schedules or automated controls in place at the same time. It is considered an override if the device has a predefined schedule that is active. This is typically the most recent action triggered on the device, such as setting the device to away mode, changing the settings manually, or
  • Modo ausente

    Plenum Airzone e Aidoo Pro - Ar condicionado – Guia do utilizador do dispositivo Wiser Home

    Modo ausente Modo ausente Modo ausente O modo ausente permite-lhe configurar os seus dispositivos inclusivamente quando não estiver em casa. Por exemplo, pode definir a temperatura e ligar/desligar os dispositivos conforme necessário. Consulte o Away Mode para obter informações detalhadas de acordo
  • Device

    Wiser Home Essential API – User Guide

    Device Device Device The following topics are examples of fetching a list of devices, device details, and the away mode status.
  • LED Indications

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

    thermostat is heating when the setpoint is higher than the current room temperature. Heating input has been activated. Away mode Status User Interaction Description Away mode is set in Wiser Home app. A dot-matrix display glows, indicates that the thermostat is in away mode.Refer Away mode
  • Understanding Control Mode Priorities

    Wiser Home – System User Guide (Germany, Austria)

    schedule. Scenario 2: You have a predefined schedule for your living room light to turn on every day at 6 PM and turn off at 10 PM. You have also set the living room light to turn Off when in away mode. At 7 PM, you leave home unexpectedly and activate Away Mode for an emergency. Response: The Away Mode overrides the predefined schedule and turns Off the living room light until the next trigger.
  • Understanding Control Mode Priorities

    Wiser Home – System User Guide (Spain and Portugal)

    schedule. Scenario 2: You have a predefined schedule for your living room light to turn on every day at 6 PM and turn off at 10 PM. You have also set the living room light to turn Off when in away mode. At 7 PM, you leave home unexpectedly and activate Away Mode for an emergency. Response: The Away Mode overrides the predefined schedule and turns Off the living room light until the next trigger.
  • Creating an automation

    EVlink Home Smart – Wiser Home device user guide

    Add conditions (C) and select any of the following (D): Device status change (Select the device) Away Mode (Enable or Disable) Energy Price changes (To define the energy price limit.) This condition is available only if your tariff is set to Peak/Off-Peak or Dynamic. Refer to Setting Tariff. Maximum
  • Creating an automation

    Wiser Micro Module Light Switch – Wiser Home Device user guide

    be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn On the lights, close the shutter etc. Refer to the Away Mode topic in the respective System User
  • Creating an automation

    System M and System D - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. For more information about Away Mode, refer to the
  • Creating an automation

    Exxact - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. For more information about Away Mode, refer to the
Page 12 of 146