DUG_EVlink_WH-07

Creating an automation

The following is an example of creating an automation to start the EVlink Home Smart when you are away.
NOTE: EVlink Home Smart can only act as an action.
  1. On the Home page, tap .
  2. Go to Automation and then tap to create an automation.
  3. Tap and choose an icon that best represents your automation.
  4. Enter a name of the automation (A) and select any of the following conditions to meet (B).
    • All conditions: All conditions must be met to trigger an automation
    • Any condition: Any one of the condition must be met to trigger an automation.
  5. Tap Add conditions (C) and select any of the following (D):
    • Device status change (Select the device)
    • Away Mode (Enable or Disable)
    • Energy Price changes (To define the energy price limit.)
      NOTE: This condition is available only if your tariff is set to Peak/Off-Peak or Dynamic. Refer to Setting Tariff.
    NOTE: Maximum 10 conditions can be added.

  6. Select Enabled mode away (E).

    NOTE: To remove an added condition, swipe left and tap .
  7. To add an action, tap Then > Add an action and select any of the following. In this case, Control a device (F).
    NOTE: Maximum 10 actions can be added.
    • Control a device: Select a device that you want to trigger.

    • Send notification: Turn on the notification for the automation.

    • Activate a moment: Select the moment that you want to trigger.

    • Wait: This option allows you to add a delay in an automation sequence. You can set the wait time in increments of 1 hour and 1 minute, up to a maximum of 24 hours. This feature is useful for delaying actions within an automation.

  8. Select EVlink Home Smart (G) and then select an action (H) to assign.
  9. Tap Save (I).
    The saved Automation is displayed on the Automation page. Tap the toggle switch on the Automation page to enable/disable the Automation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?