Showing 1,191 - 1,200 of 1,449 results

Page 120 of 145
  • Wiser temperatur och luftfuktighetssensor Bruksanvisning för Wiser Home-enhet

    ://www.productinfo.schneider-electric.com/wiser_home/search?maxFacetValues=10&filter=-search-hidden_md%3Atrue&term=Away+Mode 5. Tryck på Ändring av enhetens status > Temperatur-/luftfuktighetssensor> Temperatur. Ställ in temperaturen med skjutreglaget (D) och välj villkoret(E) (mindre än/mer än), tryck sedan på
  • Exxact – Rörelsedetektor med tryckknapp 10 A uppkopplad Bruksanvisning för Wiser Home-enhet

    https://www.productinfo.schneider-electric.com/wiser_home/search?maxFacetValues=10&filter=-search-hidden_md%3Atrue&term=Away+Mode RöststyrningMed hjälp av Amazon Alexa™ eller Google Home kan du styra enheten medrösten. FÖRSLAG: Använd det enhetsnamn som du tilldelade under parkopplingen.Till exempel
  • Seasonal Comfort-tila määrittäminen

    Wiser verhomoduuli ZB – Wiser Home -laitteen käyttöopas

    liiketunnistin on suunnattu lattiaa kohti eikä aurinkoa kohti. Seasonal Comfort-tila asetetaan seuraavasti: Napauta Home -näytössä Smart Modes Seasonal Comfort Mode. Seasonal Comfort-tila tiedot näytetään. Pyyhkäise vasemmalle nähdäksesi lisätietoja ja napauta Seuraava Jatka aloittaaksesi kausittaisen
  • Technical Data

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    Technical Data Technical Data Technical Data Nominal voltage: AC 230 V ~, 50 Hz Power consumption In standby mode (Psm) : 0.24 W In networked standby (Pnsm) : 0.32 W Networked standby with display (P) : 0.5 W Type of temperature control: TW = Electronic room temperature control plus week timer This
  • Mureva EVlink

    29 70 00 www.se.com Schneider Electric Tarif Tarif Réglez le tarif dans l'application Wiser Home pour voir les coûts énergétiques et les informations de facturation. Schneider Electric 35 rue Joseph Monier 92500 Rueil-Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric Mode de
  • Wiser Hub 2nd Generation

    Wiser Home – System User Guide (France)

    latest version, you will be prompted to update before proceeding with the setup. Put the Hub into setup-mode as per the instruction provided by the app. Then tap Next (A). Connect your smartphone to the Hub’s temporary Wi-Fi ® network either by QR Code connection or Manual connection. If you cannot
  • Room setting

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

    between a room being occupied and then transitioning to an unoccupied state.his delay ensures that the system doesn't immediately switch to an unoccupied mode when a room becomes vacant, preventing unnecessary fluctuations and providing a grace period in case the room becomes occupied again shortly
  • Room setting

    Odace - Connected Thermostat 2 A – Wiser Home Device user guide

    between a room being occupied and then transitioning to an unoccupied state.his delay ensures that the system doesn't immediately switch to an unoccupied mode when a room becomes vacant, preventing unnecessary fluctuations and providing a grace period in case the room becomes occupied again shortly
  • Création d’un automatisme

    Mureva EVlink – Guide de l'utilisateur de l'appareil domestique Wiser

    déclencher un automatisme. Appuyez sur Ajouter des conditions (C) et sélectionnez l’une des options suivantes (D) : Changement d’état d’un équipement (sélectionnez l’appareil) Mode Absence (activez ou désactivez) Changements de prix de l'énergie (Pour définir la limite de prix de l'énergie.) Cette condition
  • Setting Tariff

    Wiser Home – System User Guide (Denmark)

    change charging mode from Wiser Home AI to Charge Now or Manual or Customized Schedule. Feed in tariff: Feed in tariff will be shown only if you have set the PowerTag for Solar or Solar and Battery which feed electricity to the Grid.The electricity generated from solar or solar and battery that is
Page 120 of 145