Showing 1,211 - 1,220 of 1,648 results

Page 122 of 165
  • Réglage de la luminosité sur le variateur

    Wiser micromodule multifilaire pour variateur LED – Guide d'utilisation de l'appareil Wiser Home

  • List of Rooms

    Wiser Home – System User Guide (France)

    List of Rooms List of Rooms List of Rooms In the Rooms page, you can find all your Rooms in a condensed list. You can add new Rooms. Tap a Room in the list to navigate to the Room options. On the Setting menu: Tap Rooms (A). List of Rooms: When calculating the number of Devices in a Room, each Climate Device of a Climate control will be counted individually. For certain multi-gang Devices, each gang will be counted as a single Device.
  • Notifications and Alarms

    Wiser Home – System User Guide (UK, Ireland)

    notifications of a device in the device options. PERSONAL Overconsumption The app will trigger an alarm when the device's usage exceeds the set limit, helping you to manage and reduce overconsumption effectively. Refer to Setting-up Overconsumption Alarm for information on how to set the overconsumption alarm
  • Configuring UFH actuator

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    located. Enable toggle switch (D), if you want monitor the floor temperature using UFH floor sensor. To change the UFH channel room refer Assigning a channel to the room. Only one UFH floor sensor can be assigned to a room if you want to update refer Setting Floor Sensor Location. Tap Submit. The
  • Configurar alarme Sem consumo

    Wiser Home – Guia do Utilizador do Sistema (Espanha e Portugal)

  • Inställning av larm om ingen förbrukning

    Wiser Home – Systemanvändarhandbok (Sverige, Finland)

  • Amazon Alexa

    Wiser Home – System User Guide (Spain and Portugal)

    setpoint change if that change is to occur in under an hour. After that it goes back to its original setting, and you must tell Alexa to do it again. If a Device is following a Schedule, any setting changed by Alexa will last until the next event in the Schedule. If the Device is running in manual mode
  • Amazon Alexa

    Wiser Home – System User Guide (Sweden, Finland)

    setpoint change if that change is to occur in under an hour. After that it goes back to its original setting, and you must tell Alexa to do it again. If a Device is following a Schedule, any setting changed by Alexa will last until the next event in the Schedule. If the Device is running in manual mode
  • Configuring UFH actuator

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    located. Enable toggle switch (D), if you want monitor the floor temperature using UFH floor sensor. To change the UFH channel room refer Assigning a channel to the room. Only one UFH floor sensor can be assigned to a room if you want to update refer Setting Floor Sensor Location. Tap Submit. The
  • Configuring the device

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

    or 16 A), or Temperature & Humidity Sensor), the system calculates the average temperature measured from the devices to control the heating based on the overall temperature of the room.For more details, refer to the Setting the device as temperature source.
Page 122 of 165