Wiser HubR (1st Generation)
Using app as a Professional Installer or Home Owner:
-
Select your hub in the app. Tap HubR (A).
NOTE: If no firmware is saved in the app, you will be asked if you want to download the latest firmware. -
Put the Controller into setup-mode as per the instruction provided by the app. Then tap Next (A).
-
Navigate to your smartphone’s settings or tap Open Wi-Fi Settings (C).
-
Connect to the Hub Wi-Fi® and enter the password located on the front cover and inside the rear cover of the Hub.
-
Return to the Wiser Home App and tap Continue (D) to establish the connection.
NOTE: The Continue (D) button is enabled only after joining the Hub Wi-Fi network. -
Select your options from the Device Details screen of the HubR and tap Next.
-
Heat Source Type (A): Tap and select the type of heating system available in your home from the drop-down, and then tap OK.
-
Gas Boiler (cycle time: 10 min)
-
Oil Boiler (cycle time: 20 min)
-
Electric Boiler (cycle time: 5 min)
-
Heat Pump (cycle time: 20 min)
-
-
Boiler Type (B): Tap and select the type of control your heating system uses, and then tap OK.
-
Standard: Select this option if your heating system uses the basic On/Off control. Standard controls typically use simple On/Off commands to control the boiler. The thermostat signals the boiler to turn On when heating is needed and to turn Off when the desired temperature is reached.
-
OpenTherm: Select this option if your heating system supports OpenTherm. OpenTherm is a digital communication protocol that allows continuous communication between the boiler and thermostat. As a result, the boiler can determine the room’s current temperature and heat accordingly as required, thereby improving energy efficiency and providing more consistent heating.
NOTE: The Wiser system currently supports OpenTherm only when used with a combi boiler and a one‑channel HubR. -
-
If you choose OpenTherm control type, following additional options will appear:
-
Tap
(C) and select the Control Type your heating system uses:
Opentherm modulation -
Adjusts the water temperature from the boiler continuously to maintain your desired room temperature.
-
Keeps the boiler ON longer but uses a lower water temperature for better energy efficiency and comfort.
ON/OFF load compensation -
Adjusts how long the boiler runs to achieve the desired temperature. It runs the boiler at higher water temperatures for shorter periods.
-
Runs the boiler at higher water temperatures for shorter periods, providing faster heating.
-
-
-
-
If you want to check if the Hub has the latest version of firmware or complete the installation process without connecting to the network, tap Skip (F) and continue with chapter Updating the firmware
NOTE:-
The Skip (F) option is not available if you login to the app as a Home Owner. Refer to Roles in the Wiser Home App to find more information on the access levels.
-
The Professional Installer has the ability to skip the Wi-Fi® setup and complete the installation process. However, this means you won't be able to connect the hub to Wi-Fi®, register for an account, or control your devices outside of your home.
-
-
To connect the hub with your Wi-Fi® network and continue the setup, tap Continue (G) and continue with chapter Connecting to Wi-Fi®.