Showing 1,241 - 1,250 of 1,648 results

Page 125 of 165
  • Notifications and Alarms

    Wiser Home – System User Guide (Sweden, Finland)

    the set limit, helping you to manage and reduce overconsumption effectively. Refer to Setting-up Overconsumption Alarm for information on how to set the overconsumption alarm. No Consumption The app will trigger an alarm when the device consumes 0 watts for a set period of time. Refer to Setting-up No Consumption Alarm for information on how to set the no consumption alarm.
  • Notifications and Alarms

    Wiser Home – System User Guide (Denmark)

    the set limit, helping you to manage and reduce overconsumption effectively. Refer to Setting-up Overconsumption Alarm for information on how to set the overconsumption alarm. No Consumption The app will trigger an alarm when the device consumes 0 watts for a set period of time. Refer to Setting-up No Consumption Alarm for information on how to set the no consumption alarm.
  • Odace - Connected Blind Control Switch

    Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Setting the configure duration Setting the configure duration Each shutter motor varies in the time it takes to complete the opening/closing movement (i.e., edge to edge). Therefore, the opening/closing time of the shutter must be determined in the app
  • Configuring the device

    Odace - Connected Thermostat 2 A – Wiser Home Device user guide

    or 16 A) or Temperature & Humidity Sensor), the system calculates the average temperature measured from the devices to control the heating based on the overall temperature of the room.For more details, refer to the Setting the device as temperature source.
  • Configuring the device

    Wiser Room Thermostat – Wiser Home Device user guide

    Sensor), the system calculates the average temperature measured from the devices to control the heating based on the overall temperature of the room. For more details, refer to the Setting the device as temperature source.
  • Configuring the device

    Wiser Underfloor Heating Controller / Connection Strip – Wiser Home Device user guide

    ; Humidity Sensor), the system calculates the average temperature measured from the devices to control the heating based on the overall temperature of the room.For more details, refer to the Setting the device as temperature source.
  • System M y Sistema D - Toma de corriente inteligente, 1 elemento, 16 A

    del sistema por debajo de un límite definido. El valor límite lo establece la potencia contratada, consulte Setting Tariff. Los dispositivos que cumplan con los requisitos se añadirán automáticamente a la gestión de cargas. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison Francia +33 (0
  • Wiser Smoke Alarm - 230 V

    www.se.com Schneider Electric Setting up connection without Wiser Hub Setting up connection without Wiser Hub Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric Interconnecting devices without Wiser Hub Interconnecting devices
  • LK FUGA® Wiser wireless double relay

    configure the relay switch according to your preferences. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Setting the device location Setting the device location You can add your device to any room (such as bedroom, living room, dining room etc
  • Technical Data

    Wiser Room Thermostat – Wiser Home Device user guide

    Technical Data Technical Data Technical Data Power supply 2 alkaline batteries type IEC LR6 1.5 V (AA) Interfaces User: TFT screen, touch buttons Wiring No cabling required Temperature setting range 5 °C to 30 °C Temperature resolution 0.5 °C Operating temperature 0 °C to 45 °C Storage temperature
Page 125 of 165