DUG_Room Thermostat_WH-09

Configuring the device

IMPORTANT: The temperature data from the sensor will be used as an input for the heating system of the room. If a room has multiple temperature measuring devices (Room Thermostat,Connected Thermostat (2A or 16A), orTemperature & Humidity Sensor), the system calculates the average temperature measured from the devices to control the heating based on the overall temperature of the room. For more details, refer to the Setting the device as temperature source.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?