Wiser Motion Sensor – Wiser Home Device user guide
) → → (3 sec) → Indicates the pairing mode after function key is pressed 3 times within 1 second. If pairing is not successful, the amber LED is On for 3 seconds and then turns Off. Green LED is On for 3 seconds → (3 sec) → Pairing was successful. If already paired Action LED Indication Status Green
refer to pairing the device with Wiser Hub. LED Indications in Quick Home ConnectPairing the device in Quick Home Connect User Action LED Indication Status Press the push button 5 times in quicksuccession. LED blinks green, once per second. Pairing mode is active for 60 seconds. Whenpairing is
Wiser Home – Guide de l’utilisateur du système (France)
la pièce pour chauffer ou refroidir jusqu’à la température définie ; la ligne noire indique la température définie (cible), c’est-à-dire l’horaire de chauffage de la pièce par Wiser (en mode Auto) ou la température définie sélectionnée manuellement (en mode Manuel). Cette ligne indique la
would liketo set below Moment Action CANCEL 32 DUG_Exxact_Wireless Switch_WH-04 Exxact – Connected Wireless Switch 1-gang/2-gang Select Moment Select Moment Please select the Moment you want toassign to the top right gang switch. Away ModeBoost All Cancel all overrides Bienvenue Balcony Movie night
foispar seconde. Le mode d’appairage est actif pendant60 secondes. Lorsque l’appairage est terminé, levoyant arrête de clignoter. Dépannage dans Quick Home Connect Symptôme Cause possible Solution La LED s’allume en orange surl’appareil. L’appairage n’est pas terminé et revient auxparamètres d’usine
the device location Setting the device location You can add your device to any room (such as bedroom, living room, dining room etc.). Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric Selecting the operating mode Selecting the
enable automation.– Away Mode: Enable / Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger to turn off the lights,dimmer or closing the shutter etc. For more information refer to Awaymode. – Energy price changes: To define the energy price limit.NOTE: This condition
any of the following (C): – Device status change: To select a device to enable automation.– Away Mode: Enable / Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger to turn off the lights,dimmer or closing the shutter etc. For more information refer to Awaymode
Quick Home Connect User Action LED Indication Status Press the push button 5 times in quicksuccession. LED blinks green, once per second. Pairing mode is active for 60 seconds. Whenpairing is completed, LED stops blinking. Troubleshooting in Quick Home Connect Symptom Possible cause Solution LED
unidade de ACpermanece ligada no modo de baixo consumo (modo de espera). – Modo de impulso : O modo Impulso irá aplicar um impulso de +2 °Cdurante uma hora em cada divisão do sistema. Para obter maisinformações sobre os diferentes modos, consulte BoostMode. – Modo automático :(Este modo está