Showing 1,291 - 1,300 of 1,622 results

Page 130 of 163
  • Wiser Hub 2nd Generation

    Wiser Home – System User Guide (Germany, Austria)

    latest version, you will be prompted to update before proceeding with the setup. Put the Hub into setup-mode as per the instruction provided by the app. Then tap Next (A). Connect your smartphone to the Hub’s temporary Wi-Fi ® network either by QR Code connection or Manual connection. If you cannot find
  • Wiser Hub 2nd Generation

    Wiser Home – System User Guide (Spain and Portugal)

    latest version, you will be prompted to update before proceeding with the setup. Put the Hub into setup-mode as per the instruction provided by the app. Then tap Next (A). Connect your smartphone to the Hub’s temporary Wi-Fi ® network either by QR Code connection or Manual connection. If you cannot find
  • Room setting

    Wiser Flush-mounted Thermostat 2 A – Wiser Home Device user guide

    between a room being occupied and then transitioning to an unoccupied state.his delay ensures that the system doesn't immediately switch to an unoccupied mode when a room becomes vacant, preventing unnecessary fluctuations and providing a grace period in case the room becomes occupied again shortly
  • Wiser Hub 2nd Generation

    Wiser Home – System User Guide (UK, Ireland)

    latest version, you will be prompted to update before proceeding with the setup. Put the Hub into setup-mode as per the instruction provided by the app. Then tap Next (A). Connect your smartphone to the Hub’s temporary Wi-Fi ® network either by QR Code connection or Manual connection. If you cannot
  • Assigning a shutter group to the Wireless switch

    LK FUGA Wiser wireless battery 4 button switch – Wiser Home Device User Guide

    group and tap Save. If the device is in sleep mode, press the top-left push button on the Wireless switch 3 times to wake up the device. Then tap Confirm in the app to apply the settings. For more information, refer to Wake up the device. Each group can include up to 60 devices. You can create a
  • Adding a Schedule

    Wiser Home – System User Guide (France)

    , a default schedule is created when climate devices are assigned. When signed in as a Professional Installer: In the Device Control Screen, the Follow schedule toggle is Off by default. All rooms are set to Manual mode. You can enable the Follow schedule toggle if you want the default heating
  • Adding a Schedule

    Wiser Home – System User Guide (Sweden, Finland)

    default schedule is created when climate devices are assigned. When signed in as a Professional Installer: In the Device Control Screen, the Follow schedule toggle is Off by default. All rooms are set to Manual mode. You can enable the Follow schedule toggle if you want the default heating schedule to
  • Dépannage

    Climatiseur Airzone Plénum et Aidoo Pro – Guide de l'utilisateur de l’appareil Wiser Home

    mode de refroidissement affiche une erreur en tentant de suivre le programme horaire. Cause possible :Erreur de connexion, vos modifications ne sont peut-être pas sauvegardées dans le contrôleur. Solution :Activez un programme de refroidissement. Consultez le paragraphe Création d’un programme.
  • Adding a Schedule

    Wiser Home – System User Guide (Spain and Portugal)

    default schedule is created when climate devices are assigned. When signed in as a Professional Installer: In the Device Control Screen, the Follow schedule toggle is Off by default. All rooms are set to Manual mode. You can enable the Follow schedule toggle if you want the default heating schedule to
  • Adding a Schedule

    Wiser Home – System User Guide (Denmark)

    default schedule is created when climate devices are assigned. When signed in as a Professional Installer: In the Device Control Screen, the Follow schedule toggle is Off by default. All rooms are set to Manual mode. You can enable the Follow schedule toggle if you want the default heating schedule to
Page 130 of 163