System User Guide Wiser Home (Germany, Austria) - 14

Wiser Hub 2nd Generation

Using app as a Professional Installer or Home Owner:

  1. Select your hub in the app. Tap Hub 2nd Gen .

    NOTE: If you have logged in as a Professional Installer, the app checks for the latest firmware. If the hub is not on the latest version, you will be prompted to update before proceeding with the setup.
  2. Put the Hub into setup-mode as per the instruction provided by the app. Then tap Next (A).

  3. Connect your smartphone to the Hub’s temporary Wi-Fi® network either by QR Code connection or Manual connection.

    TIP: If you cannot find the password, tap I can’t find the password to open the Schneider Electric FAQ site in your browser.

    QR Code Connection:

    1. Tap on Open Camera and scan the QR Code from the device.

      IMPORTANT: Allow the app to access your camera when prompted.
    2. A pop-up will appear, requesting permission to use a temporary WiFi network. Tap Connect to establish the connection.

    Manual Connection:

    1. Tap on Connect Manually.

    2. Navigate to your smartphone’s settings or tap Open Wi-Fi Settings (C).

    3. Connect to the Hub Wi-Fi® and enter password located on the front cover and inside the rear cover of the Hub.

    4. Return to the Wiser Home App and tap Continue (D) to establish the connection.

  4. If you want to check if the Hub has the latest version of firmware or complete the installation process without connecting to the network, tap Skip (F) and continue with chapter Updating the firmware

    NOTE:
    • The Skip (F) option is not available if you login to the app as a Home Owner. Refer to Roles in the Wiser Home App to find more information on the access levels.

    • The Professional Installer has the ability to skip the Wi-Fi® setup and complete the installation process. However, this means you won't be able to connect the hub to Wi-Fi®, register for an account, or control your devices outside of your home.

  5. To connect the hub with your Wi-Fi® network and continue the setup, tap Continue (G) and continue with chapter Connecting to Wi-Fi®.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?