Showing 1,361 - 1,370 of 9,870 results

Page 137 of 987
  • Deleting a Schedule

    Wiser Home – System User Guide (Sweden, Finland)

    Deleting a Schedule Deleting a Schedule Deleting a Schedule On the Schedule details screen: Tap Delete (A). The Wiser Home App automatically creates a default Schedule for Climate control devices. If the Wiser Hub has to be reset, the Wiser Home app will again create a default Schedule for all
  • Editing a Schedule

    Wiser Home – System User Guide (UK, Ireland)

    Editing a Schedule Editing a Schedule Editing a Schedule In the Schedule details screen: Tap (A) icon to change the name of the Schedule. Select the Devices (B) the Schedule applies to. Select the day (C) you want to add or edit events. Tap (D) icon to edit an event. Tap (E) icon to add an event to
  • Adding a Device

    Wiser Home – System User Guide (UK, Ireland)

    Adding a Device Adding a Device Adding a Device You can add a new Device at any time. The hub must be installed before adding a Wiser device. Add mains-powered devices before battery-powered devices. Refer to Selecting the mounting location. The instructions provided for adding the device are
  • Deleting a schedule

    Exxact - Connected Multiwire Universal Push-button Dimmer LED – Wiser Home Device user guide

    Deleting a schedule Deleting a schedule Deleting a schedule On the Home screen, tap Automations Schedules. Tap the schedule you want to delete. Tap SCHEDULE DETAILS, tap Delete, and then select OK.
  • Operating a Dimmer

    Exxact - Connected Multiwire Universal Rotary Dimmer LED – Wiser Home Device user guide

    Operating a Dimmer Operating a Dimmer Operating a Dimmer You can switch the dimmer on/off and adjust its brightness using the paired Wireless switch. Short press the top or bottom of the Wireless switch (< 0,5 s) to turn on/off the connected load (A). Long press the top or bottom of the Wireless switch (> 0,5 s) to increase or decrease the brightness of the connected load (B).
  • Editing a schedule

    Exxact - Connected Blind Control Switch – Wiser Home Device user guide

    Editing a schedule Editing a schedule Editing a schedule On the Home screen, tap Automations Schedules. Tap the schedule you want to edit. Tap the SCHEDULE DETAILS and you can do the following actions: Rename the schedule (A). Within the Applies to (B) menu, you have the option to select from the
  • Deleting a schedule

    LK FUGA Wiser Multiwire LED Rotary Dimmer – Wiser Home Device User Guide

    Deleting a schedule Deleting a schedule Deleting a schedule On the Home screen, tap Automations Schedules. Tap the schedule you want to delete. Tap SCHEDULE DETAILS, tap Delete, and then select OK.
  • Deleting a Schedule

    Wiser BMS – Building Management System – User Guide

    Deleting a Schedule Deleting a Schedule Deleting a Schedule Select a room in the floorplan layout. The selected room screen appears. Click Schedule. The Wiser Schedule screen appears. On the Wiser Schedule screen, click Edit Click Delete. The event will be removed from the Schedule Details page.
  • Editing a schedule

    Odace - Connected Multiwire Universal Push-button Dimmer LED – Wiser Home Device user guide

    Editing a schedule Editing a schedule Editing a schedule On the Home screen, tap Automations Schedules. Tap the schedule you want to edit. Tap the SCHEDULE DETAILS and you can do the following actions: Rename the schedule (A). Within the Applies to (B) menu, you have the option to select from the
  • Editing a schedule

    LK One Wiser Push-button Switch – Wiser Home Device user guide

    Editing a schedule Editing a schedule Editing a schedule On the Home screen, tap Automations Schedules. Tap the schedule you want to edit. Tap the SCHEDULE DETAILS and you can do the following actions: Rename the schedule (A). Within the Applies to (B) menu, you have the option to select from the
Page 137 of 987