SUG_SV_FI_WH-04

Deleting a Schedule

On the Schedule details screen:

  1. Tap Delete (A).

    NOTE: The Wiser Home App automatically creates a default Schedule for Climate control devices.

    If the Wiser Hub has to be reset, the Wiser Home app will again create a default Schedule for all Climate Control devices once assigned to the room.

    To not follow the Schedule, remove the Device from the Applies to list in schedule details or disable the Follow schedule toggle switch in the Climate control/Device control page.

    It is recommended to not delete a default Climate Schedule.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.