Showing 1,401 - 1,410 of 1,622 results

Page 141 of 163
  • Climatiseur Airzone Plénum et Aidoo Pro

    + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric ModeAbsence ModeAbsence Le mode Absence vous permet de configurer vos appareils lorsque vous êtes loin de chez vous. Par exemple, vous pouvez définir la température et mettre en marche/arrêter les appareils si nécessaire. Reportez-vous à la
  • Pairing the device with the Wiser Hub

    Mureva EVlink – Wiser Home Device User Guide

    Pairing the device with the Wiser Hub Pairing the device with the Wiser Hub Pairing the device with the Wiser Hub Pair your EV Socket with the Wiser Hub to access and control it using the Wiser Home app. Make sure that the EV Socket is installed by an electrician. Must use Mode 2 cable (max 16 A
  • Exxact - Connected Double Socket Outlet 16A Wiser Home Device user guide

    - Connected Double Socket Outlet 16A 4. Tap Add conditions (B) and select any of the following (C). – Device status change (Select the device): An automation will be triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable
  • Criar uma automatização

    Plenum Airzone e Aidoo Pro - Ar condicionado – Guia do utilizador do dispositivo Wiser Home

    ) para definir a condição. Se tiver selecionado a condição como Modo ausente e a ação como Controlar um dispositivo, esta automatização irá sobrepor-se às definições do Away Mode. Selecione as opções que pretende configurar: Toque em (F) e arraste a barra deslizante para cima/baixo (G) para ajustar a
  • Couplage de l’appareil avec la passerelle Wiser

    Mureva EVlink – Guide de l'utilisateur de l'appareil domestique Wiser

    installée par un électricien. Vous devez utiliser le câble Mode 2 (max 16 A - 3.7 kW) pour charger votre voiture à partir de la EV Prise. Sur l’écran d’ Accueil, appuyez sur . Plot Dispositifs Énergie Prise Mureva EVlink. Vous pouvez également naviguer en appuyant sur Contrôle > > Énergie > Prise
  • Wiser Home AI

    Wiser Home – System User Guide (Sweden, Finland)

    to activate or deactivate loads. Temporary Override Function (Away Mode): Overrides the Wiser Home AI function to adapt your home settings when you are away, ensuring energy efficiency even when you're not home. Notifications for Feature Malfunction: Notifies you in case of a feature malfunctions
  • Wiser BMS – Building Management System User Guide

    BSystem of measurementInternational System of Units (metric) ADate, time and number formatAuto LanguageAuto E User settings OnAutoRelative timeE OnAuto 20 UG_Wiser Building Management System_WH-00 Wiser Building Management System Theme Settings Dark Mode (F) Allows you to set the interface to a dark
  • Unica - Connected Single Socket Outlet 16 A Wiser Home Device user guide

    quicksuccession. LED blinks green, once per second. Pairing mode is active for 60 seconds. Whenpairing is completed, LED stops blinking. Troubleshooting in Quick Home Connect Symptom Possible cause Solution LED displays amber on the device. Pairing not completed and returned to factorydefault. Pair the
  • Ovalis - Connected Single Socket Outlet 16 A Wiser Home Device user guide

    quicksuccession. LED blinks green, once per second. Pairing mode is active for 60 seconds. Whenpairing is completed, LED stops blinking. Troubleshooting in Quick Home Connect Symptom Possible cause Solution LED displays amber on the device. Pairing not completed and returned to factorydefault. Pair the Wireless
  • Wiser Home AI

    Wiser Home – System User Guide (France)

    . Temporary Override Function (Away Mode): Overrides the Wiser Home AI function to adapt your home settings when you are away, ensuring energy efficiency even when you're not home. Notifications for Feature Malfunction: Notifies you in case of a feature malfunctions. Supported devices: Power
Page 141 of 163