Showing 1,411 - 1,420 of 1,648 results

Page 142 of 165
  • Pairing the device with the Wiser Hub

    System M and System D - Connected Push-button Module, 1-gang/2-gang – Wiser Home Device user guide

    slats: Proceed to step 8 and step 10. Tap Shutter Next and enter the open/close duration of shutter. Refer to Setting default run time. Tap Shutter with tilting slats Slat Type, select a slat type and tap Set: Horizontal Tilted Vertical Tap Next and enter the following durations: Open duration
  • PowerTag Wiser Home Geräte-Benutzerhandbuch

    ://www.productinfo.schneider-electric.com/wiser_home/search?maxFacetValues=10&filter=-search-hidden_md%3Atrue&term=%22Setting+Tariff%22&f.manualType_md=System+User+Guide+%28France%29&f.manualType_md=System+User+Guide+%28UK%2C+Ireland%29&f.manualType_md=System+User+Guide+%28Spain+and+Portugal%29
  • Floor sensors settings

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    temperature ranges from -9°C to +9°C and can be adjusted in 0.1°C increments. Tap Save. Floor sensor limit To set the upper and lower temperature limit: On setting page, tap Floor Sensor Upper Limit to set upper temperature limit of the floor sensor and then tap Save. The temperature ranges form 5
  • Floor sensors settings

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    temperature ranges from -9°C to +9°C and can be adjusted in 0.1°C increments. Tap Save. Floor sensor limit To set the upper and lower temperature limit: On setting page, tap Floor Sensor Upper Limit to set upper temperature limit of the floor sensor and then tap Save. The temperature ranges form 5
  • Using the device

    LK FUGA® Wiser wireless PIR dimmer with neutral – Wiser Home Device user guide

    information, refer to Setting up a schedule. E Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide. F Tap to open the History screen, which displays previously recorded motion detection
  • Unica - Toma de corriente inteligente, 1 elemento, 16 A

    sistema por debajo de un límite definido. El valor límite lo establece la potencia contratada, consulte Setting Tariff. Los dispositivos que cumplan con los requisitos se añadirán automáticamente a la gestión de cargas. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison Francia +33 (0) 1
  • Using the device

    Exxact - Connected Motion Sensor with Push-button Dimmer LED – Wiser Home Device user guide

    information, refer to Setting up a schedule. E Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide. F Tap to open the History screen, which displays previously recorded motion detection
  • About the device

    Wiser Smart Plug 16A – Wiser Home Device User Guide

    the Wiser app you will need the Wiser Hub. Direct operation: The plug can always be controlled directly on-site. To do this, you can switch the plug On and Off with the operation button. Functions Switching On and Off plugged-in devices manually and remotely via app. Setting a timer or a time
  • Wiser Passerelle avec Relais 2e Génération

    Wiser Home – Guide de l’utilisateur du système (France)

  • Wiser UP-Lastaktor Geräte-Benutzerhandbuch

    ://www.productinfo.schneider-electric.com/wiser_home-dev2/search?maxFacetValues=10&filter=-search-hidden_md%3Atrue&term=SETTING+TARIFF https://www.productinfo.schneider-electric.com/wiser_home-dev2/search?maxFacetValues=10&filter=-search-hidden_md%3Atrue&term=anti+tripping+management EnergiezentraleSie können Ihren
Page 142 of 165