DUG_LK FUGA Wiser wireless PIR dimmer with neutral_WH-01

Using the device

The Device Control Screen allows you to switch on/off, adjust the brightness level and control various settings.

On the Control tab, select Motion Sensor Dimmer.

The Device Control Screen displays the following options:

A

Tap to turn the device on/off.

B

Drag the slider bar up/down to increase/decrease the brightness of your motion dimmer. For more information, refer to Adjusting the brightness.

C

Displays the current Lux value of the light present in the room.

D

Tap to open the Schedule screen, where you can create a schedule. For more information, refer to Setting up a schedule.

E

Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide.

F

Tap to open the History screen, which displays previously recorded motion detection events, including the date, time, and status of each event. For more information, refer to History.

G

Tap to open the Device Settings screen and configure the settings. For more information, refer to Configuring the device.

H

Displays the current motion detection state, such as:

  • Occupied: Motion is detected.

  • Unoccupied: No motion is detected.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.