Showing 1,411 - 1,420 of 1,622 results

Page 142 of 163
  • Wiser Home

    Electric 35 rue Joseph Monier 92500 Rueil Malmaison Frankrig + 33 (0) 1 41 29 70 00 www.se.com Væk-tilstand Væk-tilstand Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison Frankrig + 33 (0) 1 41 29 70 00 www.se.com Boost-tilstand Boost-tilstand Schneider Electric 35 rue Joseph Monier 92500 Rueil
  • Wiser Home AI

    Wiser Home – System User Guide (France)

    . Temporary Override Function (Away Mode): Overrides the Wiser Home AI function to adapt your home settings when you are away, ensuring energy efficiency even when you're not home. Notifications for Feature Malfunction: Notifies you in case of a feature malfunctions. Supported devices: Power
  • Couplage de l’appareil avec la passerelle Wiser

    Mureva EVlink – Guide de l'utilisateur de l'appareil domestique Wiser

    installée par un électricien. Vous devez utiliser le câble Mode 2 (max 16 A - 3.7 kW) pour charger votre voiture à partir de la EV Prise. Sur l’écran d’ Accueil, appuyez sur . Plot Dispositifs Énergie Prise Mureva EVlink. Vous pouvez également naviguer en appuyant sur Contrôle > > Énergie > Prise
  • Wiser Home AI

    Wiser Home – System User Guide (Sweden, Finland)

    to activate or deactivate loads. Temporary Override Function (Away Mode): Overrides the Wiser Home AI function to adapt your home settings when you are away, ensuring energy efficiency even when you're not home. Notifications for Feature Malfunction: Notifies you in case of a feature malfunctions
  • Unica - Connected Single Socket Outlet 16 A Wiser Home Device user guide

    quicksuccession. LED blinks green, once per second. Pairing mode is active for 60 seconds. Whenpairing is completed, LED stops blinking. Troubleshooting in Quick Home Connect Symptom Possible cause Solution LED displays amber on the device. Pairing not completed and returned to factorydefault. Pair the
  • Ovalis - Connected Single Socket Outlet 16 A Wiser Home Device user guide

    quicksuccession. LED blinks green, once per second. Pairing mode is active for 60 seconds. Whenpairing is completed, LED stops blinking. Troubleshooting in Quick Home Connect Symptom Possible cause Solution LED displays amber on the device. Pairing not completed and returned to factorydefault. Pair the Wireless
  • Wiser temperatur-/fugtighedssensor Brugervejledning til Wiser Home-enheden

    /wiser_home/search?maxFacetValues=10&filter=-search-hidden_md%3Atrue&term=Away+Mode 5. Tryk på Ændring af enhedens status > Temperatur-/fugtighedssensor >Temperatur. Indstil temperaturen med skyderen (D), og vælg betingelsen (E)(mindre end/mere end), og tryk derefter på indstil. BEMÆRK: Når skyderen
  • Exxact - Connected Motion Sensor with Push-button Dimmer LED

    Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Voice control Voice control Using Amazon Alexa™ or Google Home, you can control the device with your voice. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France
  • Unica - Détecteur de mouvement avec interrupteur 10 A connecté

    Rueil-Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Activer/désactiver l’appareil à l’aide de l’application Activer/désactiver l’appareil à l’aide de l’application Schneider Electric 35 rue Joseph Monier 92500 Rueil-Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Mode Absence Mode Absence
  • Wiser Home Systembrugervejledning (Danmark)

    apparater der skal slukkes, når du har valgtVæk-tilstand SUG_DA_WH-04 107 Konfiguration af Wiser-systemet 2. Aktivér/deaktivér vippekontakten for at aktivere/deaktivere Væk-tilstanden. Boost-tilstandBoost Mode vil anvende et boost på +2 °C i en time for alle rum i systemet. På skærmen Automatisering:1
Page 142 of 163