be available. H Add or remove the device from Favourite devices. Refer to Managing Favourites J Navigate to the Room Details of the room to which the climate control is assigned. Setting up a Climate Control While setting up your Climate Control, make sure to consider the following information
with the Wiser Hub ........................................................10Configuring the device ..............................................................................13 Setting the device location ...................................................................14Setting the detection
correctly or not for EVlink Home Smart with TIC function. Device not removed from the system Hub disconnected from the network. (Applicable only for users with EVlink Home Smart and Wiser hub installed together) Charger unavailable. Device connected to another home network. Try setting up the device
par le PCM. Vous pouvez inscrire jusqu'à huit charges à lafois, ce qui permet de maintenir la consommation totale du système en dessousde la limite établie. Cette limite est déterminée par les spécifications de votrecontrat, il est donc important de consulter la section SettingTariff pour obtenir
Insight+. The Unlock Insight+ option is available only until the setup is complete. Tap Get help setting up my IHD. If you have already set up your IHD, tap I’ve already set up my IHD option. Follow the instructions in the app to set up the IHD and tap Finish once complete. Using Insight+ Using Insight
elemento, 16 A https://www.productinfo.schneider-electric.com/wiser_home/search?maxFacetValues=10&filter=-search-hidden_md%3Atrue&term=SETTING+TARIFF&f.lang_md=es Requisito previo: • Configure uno de sus dispositivos PowerTag como Red. ConsulteEmparejamiento del PowerTag principal. • Ajuste la potencia