Showing 281 - 290 of 1,648 results

Page 29 of 165
  • Setting the device location

    Setting the device location Setting the device location Setting the device location You can add your device to any room (such as bedroom, living room, dining room etc.). On the Home screen, tap . Tap Devices, select the device from the list for which you wish to change the location. Tap Location to
  • Setting the configure duration

    System M and System D - Connected Push-button Module, 1-gang/2-gang – Wiser Home Device user guide

    Setting the configure duration Setting the configure duration Setting the configure duration Each shutter motor varies in the time it takes to complete the opening/closing movement (i.e., edge to edge). Therefore, the opening/closing time of the shutter must be determined in the app. To determine
  • Setting RL-LED mode

    Wiser Micro Module Dimmer – Wiser Home Device user guide

    Setting RL-LED mode Setting RL-LED mode Setting RL-LED mode You can change the dimming mode in the app if you have problems with light flickering. By changing the dimming mode, the dimming quality is also improved. On the Home screen, tap . Tap Devices Micromodule Dimmer . Tap the toggle switch (A) to enable the RL-LED Mode.
  • Setting the threshold temperature

    Wiser Micro Module Shades Control – Wiser Home Device user guide

    Setting the threshold temperature Setting the threshold temperature Setting the threshold temperature Using the Wiser Home app, you can define the inside and outside temperature of a room above which the shutters shall close. To set the threshold inside and outside temperature: In the Seasonal Comfort Mode set-up page, tap Temperature. Set the inside and outside desired temperatures and tap Set.
  • Setting up a schedule

    Wiser Micro Module Shades Control – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule The shutter can be controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time. The devices can be fully controlled by schedule
  • Setting-up Overconsumption Alarm

    Wiser Home – System User Guide (France)

    Setting-up Overconsumption Alarm Setting-up Overconsumption Alarm Setting-up Overconsumption Alarm This topic explains how to setup an overconsumption alarm for a device. On the Notifications and Alarms screen, tap Create a new alarm (A). Choose alarm type as Overconsumption (B). Select the device
  • Setting up the Hub

    Wiser Home – System User Guide (France)

    Setting up the Hub Setting up the Hub Setting up the Hub In order to be able to control the system via your smartphone, the hub must be connected to the internet. You can set up the Hub by using the app as Home Owner and Professional Installer. The app offers the Professional Installer menu for
  • Setting the device control

      Same topic found multiple times in this document:
    Setting the device control Using the Wiser Home app, you can set the control type such as Relay or OpenTherm. To set the control type: On the Home screen, tap . Tap Devices Boiler Relay Control Type (A) to select given option: Relay OpenTherm
  • Setting up a schedule

    Ovalis - Connected Blind Control Switch – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule The shutter can be controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time. The devices can be fully controlled by schedule
  • Setting the configure duration

    Ovalis - Connected Blind Control Switch – Wiser Home Device user guide

    Setting the configure duration Setting the configure duration Setting the configure duration Each shutter motor varies in the time it takes to complete the opening/closing movement (i.e., edge to edge). Therefore, the opening/closing time of the shutter must be determined in the app. To determine
Page 29 of 165